Accessing UUID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accessing UUID

4,188件の閲覧回数
mditto1
Contributor III

I'm running on our custom LPC55S69 board.  I'm trying to access the UUID in the protected flash region.  After reading the Flash_ifr_driver section of the SDK API Reference Manual, I added the "IAP1" driver in MCUXpresso and added this code to my project:

#include "fsl_iap_ffr.h"

...

flash_config_t flash_config;
uint8_t uuid_buf[16];
printf("FFR_Init: %d\n", FFR_Init(&flash_config));
printf("FFR_GetUUID: %d\n", FFR_GetUUID(&flash_config, uuid_buf));
printf("uuid_buf: %02X %02X %02X %02X %02X %02X %02X %02X\n",
       uuid_buf[0], uuid_buf[1], uuid_buf[2], uuid_buf[3],
       uuid_buf[4], uuid_buf[5], uuid_buf[6], uuid_buf[7]);
printf(" %02X %02X %02X %02X %02X %02X %02X %02X\n",
      uuid_buf[8], uuid_buf[9], uuid_buf[10], uuid_buf[11],
      uuid_buf[12], uuid_buf[13], uuid_buf[14], uuid_buf[15]);

The code compiles and the functions return success (0) but the data is all 0xFF.

Why isn't it working?

Mike

ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

4,120件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mike,

I just add your code into "flashiap" demo under SDK, it can work well:

pastedImage_1.png

What about the version of your chip ? You can get it from the masking of chip. 

And how about use the latest SDK v2.8 and latest MCUXpresso IDE v11.2.0.

Regards,

Alice

0 件の賞賛
返信

4,120件の閲覧回数
mditto1
Contributor III

On further analysis, if I update the ConfigTools Clocks settings to enable the FRO 96M clock, then the MCUXpresso-generated code (clock_config.c) is sufficient and I don't need to copy the BOARD_BootClockFROHF96M function from the example.  I also don't seem to need to call FLASH_Init any more, just calling FFR_Init is sufficient.

I noticed that after I've successfully called FFR_Init and FFR_GetUUID, I can't free/re-use the memory where the flash_config_t object was stored because it continues to be referenced by some sort of interrupt handler, even though I am not calling any FFR or flash functions.  The SDK API reference manual mentions a function FFR_Deinit, but this function doesn't exist in the SDK header files.  I made the object static/global to get around this.

This is working well enough for me now, thanks for the help.

0 件の賞賛
返信

4,120件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

OK, thanks for your sharing.

0 件の賞賛
返信

4,120件の閲覧回数
mditto1
Contributor III

Alice,

Thanks, I tried the flashiap1 demo and it works, so I investigated what the demo had that my project was missing.  It turned out I needed two things:

Copy the BOARD_BootClockFROHF96M function from the example and call it.

Call FLASH_Init.

Now I can read the UUID.

I will study the BOARD_BootClockFROHF96M function; I assume it is doing things that really should be done in the IDE Clocks tool.

Thanks,

Mike

0 件の賞賛
返信