About LPC802 Flash memory control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LPC802 Flash memory control

Jump to solution
2,513 Views
pluorinee
Contributor II

Hello, I'm new in here.

 

I'm wondering how Flash memory works within the LPC802.

The LPC802 can operate in 15 MHz, but Flash memory isn't fast enough to.

 

I search LPC802 datasheet & User Manual, but I couldn't find about it.

Is there any technology to control Flash memory?

 

Thank you for your help.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,463 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello pluorinee,

The maximal Flash clock frequency is 15M, which is the same as maximal system clock.

Please see below statement in UM11045

ZhangJennie_0-1727250125329.png

Thanks,

Jun Zhang

 

 

View solution in original post

3 Replies
2,487 Views
pluorinee
Contributor II

Can NOR Flash of LPC802 handle a read speed of 15 MHz System clock?

And does it use technologies such as wait state to manage Flash memory when it is running?

Thank you for your help.

0 Kudos
Reply
2,463 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello pluorinee,

The maximal Flash clock frequency is 15M, which is the same as maximal system clock.

Please see below statement in UM11045

ZhangJennie_0-1727250125329.png

Thanks,

Jun Zhang

 

 

2,459 Views
pluorinee
Contributor II
Thanks for the reply
0 Kudos
Reply