About (LPC54018 OM40003) USB Power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About (LPC54018 OM40003) USB Power

Jump to solution
3,796 Views
RodrigoEngComp
Contributor I

Heyy,

 

I'm using an OM40003 board and I need to know if I can use the board with the two USB, shown in the file, connected and powered on at the same time.

 

I need both at the same time because in full operation I use a source as the main power(without using computer usb for Debug), and at another time I need to use a source and the computer for debug (passing 5 volts also from the computer's USB).

 

Best regards,

 

Rodrigo Almeida.

0 Kudos
Reply
1 Solution
3,788 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, you can use USB power this way.

View solution in original post

0 Kudos
Reply
1 Reply
3,789 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, you can use USB power this way.

0 Kudos
Reply