About (LPC54018 OM40003) USB Power

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About (LPC54018 OM40003) USB Power

ソリューションへジャンプ
3,810件の閲覧回数
RodrigoEngComp
Contributor I

Heyy,

 

I'm using an OM40003 board and I need to know if I can use the board with the two USB, shown in the file, connected and powered on at the same time.

 

I need both at the same time because in full operation I use a source as the main power(without using computer usb for Debug), and at another time I need to use a source and the computer for debug (passing 5 volts also from the computer's USB).

 

Best regards,

 

Rodrigo Almeida.

0 件の賞賛
返信
1 解決策
3,802件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, you can use USB power this way.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,803件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, you can use USB power this way.

0 件の賞賛
返信