ARM Cortex "Reserved" interrupts

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ARM Cortex "Reserved" interrupts

1,412 次查看
danielgull
Contributor IV

Hi NXP community

I have a question related to the NXP LPC54000 microcontroller family.

Here we use Cortex-M0 and Cortex-M4. These ARM cores provide interrupts.

Some interrupts are labeled as "Reserved".

Do these "Reserved" interrupts actually exist on Silicon?

If they exist on Silicon but are not mapped to any hardware can they be used as "Software" interrupts?

If they exist on Silicon are there plans to remove this hardware in the future to save silicon area to optimized?

Many thanks.

Dani

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

1,296 次查看
soledad
NXP Employee
NXP Employee

Hi, 

No, there are not mapped to any hardware however they cannot be used as "Software" interrupts?

and there is no plan to remove this.

Have a great day,

Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复