AN11080 broken link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN11080 broken link

1,711 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DPeters on Thu Oct 20 10:29:59 MST 2011
There was a tweet by lpcadmin a number of weeks ago about Application Note: AN11080 Using SPIFI with LPC1800 with software.  The link to the file isn't available.  Does anyone have the file?
Labels (1)
0 Kudos
Reply
4 Replies

1,705 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by usb10185 on Sat Dec 31 14:43:00 MST 2011
Regarding the LPC1788: It was removed since the SPIFI block was not functional. There are no plans to fix or for SPIFI support to be added to the LPC1788 family.
0 Kudos
Reply

1,705 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dave on Fri Dec 16 11:21:59 MST 2011
Is this the same for the LPC1788?  I noticed in rev 1.2 of the user's manual, they removed the SPIFI as well...
0 Kudos
Reply

1,705 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Thu Dec 15 15:05:29 MST 2011
The UM is currently being updated, and the SPIFI chapter needs to be rewritten to document the API used to access the SPI flash ... it will be back soon. :)
0 Kudos
Reply

1,705 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ian Hickey on Wed Dec 14 18:13:22 MST 2011
Worse, the entire chapter on the SPIFI is missing from the latest User manual (UM10430 v1)
http://www.lpcware.com/content/nxpfile/lpc1850302010-data-sheet

The latest datasheet v3 states in the revision history that the SPIFI driver has been removed from ROM.

0 Kudos
Reply