ADC burst mode suggestion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC burst mode suggestion

1,033件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bruno.vt on Wed Oct 15 23:48:41 MST 2014
Hello, in my application with LPC15xx I have to read about 10 analog signal.
My idea is to configure the A/D conversion in burst mode and then read the measures when I need them from the A/D Channel Data Register.
I don't need precise timings sample.
Is there any drawbacks to use burst mode?
ラベル(1)
0 件の賞賛
返信
1 返信

990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Oct 16 10:22:25 MST 2014
Hi Bruno
There should not be any disadvantage using the ADC in burst mode.

Paul
0 件の賞賛
返信