ADC burst mode suggestion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC burst mode suggestion

1,414 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bruno.vt on Wed Oct 15 23:48:41 MST 2014
Hello, in my application with LPC15xx I have to read about 10 analog signal.
My idea is to configure the A/D conversion in burst mode and then read the measures when I need them from the A/D Channel Data Register.
I don't need precise timings sample.
Is there any drawbacks to use burst mode?
Labels (1)
0 Kudos
Reply
1 Reply

1,371 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Oct 16 10:22:25 MST 2014
Hi Bruno
There should not be any disadvantage using the ADC in burst mode.

Paul
0 Kudos
Reply