12bit ADC - Simultaneous sampling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

12bit ADC - Simultaneous sampling

1,233 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by noddy14 on Fri Oct 10 08:52:04 MST 2014
Hello

I need to do simultaneous sampling of 2 analogue signals using the 12bit ADC in the LPC4370.

The data sheet shows a 6:1 MUX at the input of the ADC but I did not find a detail description so I assume the sampling is only done in the ADC block so all that can be done is sequential sampling.

Can anyone comment / confirm my understanding is correct?

Thanks!


Labels (1)
0 Kudos
Reply
1 Reply

1,200 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cb03scs on Wed Oct 22 00:17:58 MST 2014
Yes that is correct... with the 80MSps 12bit ADC only sequential sampling is possible.
0 Kudos
Reply