12bit ADC - Simultaneous sampling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

12bit ADC - Simultaneous sampling

1,282件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by noddy14 on Fri Oct 10 08:52:04 MST 2014
Hello

I need to do simultaneous sampling of 2 analogue signals using the 12bit ADC in the LPC4370.

The data sheet shows a 6:1 MUX at the input of the ADC but I did not find a detail description so I assume the sampling is only done in the ADC block so all that can be done is sequential sampling.

Can anyone comment / confirm my understanding is correct?

Thanks!


ラベル(1)
0 件の賞賛
返信
1 返信

1,249件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cb03scs on Wed Oct 22 00:17:58 MST 2014
Yes that is correct... with the 80MSps 12bit ADC only sequential sampling is possible.
0 件の賞賛
返信