At 7 minutes you mentioned needing 3.3 volts for your display. You should be able to hook up 3.3 volts on the X101 connector, pin 1. The schematic labels this VDD_TARGET. It's derived from N400 Torex XC6206P331MR-G and should be good for 200mA. LPC55S69 will take in the region 10mA and debug interface LPC11U35 takes about 12 mA.
Good information Mark. I realized this after I had gotten everything recorded. My brain was really looking for a +3.3v net label and I completely missed VDD_TARGET. +3.3v is definately availabe on the pin headers for user acces.
I have acquired the E1 board and downloaded the IDE. I have successfully completed the led_blink example. Now I am trying the hello world example and failing. Where can I turn for help? Everything built OK. My console says it is a semihosting telnet console. The debugger stopped at a breakpoint and I resumed execution. The debugger window says the program is running.
I can't find the output.
I'm running on Ubuntu 18 something.
I put a printf in the while(1) loop so it would steadily be doing something.
Now I see two commands in "top" that are using CPU:
redlinkserv crt_emu_cm_redl
So it seems to be happily doing something. It is just not showing up anywhere I can find it.
I expect that the code has hung up in the clock initialisation routine.
The LED blink example probably sets up the clocking with function call BOARD_BootClockFROHF96M().
The hello_world example probably configures the clocks with BOARD_InitBootClocks() which then calls BOARD_BootClockPLL150M().
This PLL function call initialises the 16 MHz crystal, and uses it as a reference for the PLL0. Then waits for PLL0 to lock. Only problem is that there is no 16 MHz crystal fitted to OKdo E1 board. The led_blinky project runs the chip from the fast 96MHz internal free-running oscillator without needing the PLL.
I found a happy ending. Having already been successful with led_blinky.c and the OKdo tutorial, I decided to add a printf in the timing loop. I also needed to include stdio.h at the top. And that works just fine printing a line every second.
I noticed that the hello_world examples (there are three) all seem to reference the UART in their descriptions (and SWO?). So maybe I was just picking the wrong example.
But I have terminal output now so I am a happy guy.
Thanks for your hard work on the videos and blog posts.