Which Cortex-M CPU revision is implemented in NXP microcontrollers?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which Cortex-M CPU revision is implemented in NXP microcontrollers?

2,886 次查看
lpcware-support
Senior Contributor I

CPU Core Revision

 

Background

 

The CPU core revision level is identified in the System Control Block (SCB) by the CPUID register found at address 0xE000ED00.  Further information can be found in ARM’s Device Generic User Guide.

ARM defines the structure of this register for each CPU variant.

Cortex-M0:       http://infocenter.arm.com/help/topic/com.arm.doc.ddi0432c/Bhccjgga.html

Cortex-M0+:     http://infocenter.arm.com/help/topic/com.arm.doc.ddi0484c/Bhccjgga.html

Cortex-M3:       http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0552a/CIHFDJCA.html

Cortex-M4:       http://infocenter.arm.com/help/topic/com.arm.doc.dui0553a/CIHCAGHH.html

 

Reference

 

The following devices are provided for reference.

                LPC812                 r0p0       Cortex-M0+

                LPC1768               r2p0       Cortex-M3

                LPC1788               r2p0       Cortex-M3

                LPC1837               r2p1       Cortex-M3

                LPC1850               r2p1       Cortex-M3

                LPC4357               r0p1       Cortex-M4F

 

Debugging

 

When debugging under the Keil uVision IDE, enterring "SCB" in the Memory1 view will display the contents of the CPUID register.

标签 (5)
0 回复数