What is the required accuracy for the regulator input to the LPC17xx?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the required accuracy for the regulator input to the LPC17xx?

1,716 Views
lpcware-support
Senior Contributor I

The internal voltage regulator voltage will always regulate around 1.8V where the external input voltage can range from 2.4V to 3.6V over the temperature range of -40C to 85C.

Labels (2)
Tags (2)
0 Kudos
Reply
0 Replies