What is the significance of Ethernet Symbol Error bit on LPC1768 in Receive Status Information in the User’s Manual? The description of this bit states that “The PHY reports a bit error over the PHY interface during reception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the significance of Ethernet Symbol Error bit on LPC1768 in Receive Status Information in the User’s Manual? The description of this bit states that “The PHY reports a bit error over the PHY interface during reception

2,855 Views
lpcware-support
Senior Contributor I

This is the event that occurs on ENET_RX_ER pin (P1.14), so if the PHY for some reason drove this pin high, it should (eventually) show up as a high SymbolError bit, and on Receive Status Vector bit 19. It's an indicator that the whole frame is suspect, and should be discarded. Basically, the PHY is indicating that there is an error raising the ENET_RX_ER line, and the user must investigate why the PHY is asserting this line

Labels (2)
Tags (2)
0 Kudos
Reply
0 Replies