What is the required accuracy for the regulator input to the LPC17xx?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the required accuracy for the regulator input to the LPC17xx?

2,194件の閲覧回数
lpcware-support
Senior Contributor I

The internal voltage regulator voltage will always regulate around 1.8V where the external input voltage can range from 2.4V to 3.6V over the temperature range of -40C to 85C.

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)