What is the difference between error active and error passive?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the difference between error active and error passive?

13,602 次查看
lpcware
NXP Employee
NXP Employee

CAN controllers initialize into error active state. Although this state has the word “error” in the name it doesn’t mean there is an error. It means that the CAN controller can actively send error frames if needed to indicate corrupted data. If the CAN controller is in error passive state then there is a potential problem with the controller or its connectivity and therefore it is not allowed to send error frames.

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

标签 (1)
标记 (1)
0 回复数