What is CAN-FD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is CAN-FD?

3,960 Views
lpcware
NXP Employee
NXP Employee

CAN-FD is a new CAN bus frame format, developed by Bosch. The current version was also published as
an international standard ISO 11898-1:2015. It allows for up to 64 bytes of data per frame and
significantly higher bit rates. Note that the first CAN-FD implementations are referred to as non-ISO
CAN-FD and should not be used due to flaws in the CRC handling. The ISO version of CAN-FD not only
fixes the flaws but has an increased hamming distance. With CAN-FD, nodes can transmit more data,
faster and with improved data integrity, while retaining all other features that make CAN ideal for
industrial communications.

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies