How is the transmit error counter reset?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How is the transmit error counter reset?

3,842件の閲覧回数
lpcware
NXP Employee
NXP Employee

The transmit error counter cannot be manually reset. It is part of the error detection and handling mechanism of the CAN bus. If the error counter is continually increasing then it indicates a problem with either the CAN controller, the bus or the receivers. Eventually the counter will reach 256 and the controller will enter “bus off” state. At this point the firmware needs to re-initialize the CAN controller. The fundamental problem that is causing the counter to increase should be addressed as it shouldn’t happen in normal operation.

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

ラベル(1)
  • CAN

タグ(1)
0 件の賞賛
返信
0 返答(返信)