How is the LPC2478 32-bit External Memory Controller different than the LPC1788 32-bit External Memory Controller?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How is the LPC2478 32-bit External Memory Controller different than the LPC1788 32-bit External Memory Controller?

3,092件の閲覧回数
lpcware-support
Senior Contributor I

The LPC1788 includes the same memory controller except for the addition an optional address shift mode for static memories that can simplify the board design and potentially increases external memory addressing range in some cases. The LPC1788 is pin-compatible with the LPC2478 but contains a Cortex M3 processor core instead of an ARM7.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

2,821件の閲覧回数
lpcware-support
Senior Contributor I

I think this is wrong.

According to the user manual UM10470, the 'address shift'
only applies to static ram, NOT to SDRAM (dynamic RAM).

0 件の賞賛
返信