How is the LPC2478 32-bit External Memory Controller different than the LPC1788 32-bit External Memory Controller?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How is the LPC2478 32-bit External Memory Controller different than the LPC1788 32-bit External Memory Controller?

3,200 次查看
lpcware-support
Fresh Out Contributor

The LPC1788 includes the same memory controller except for the addition an optional address shift mode for static memories that can simplify the board design and potentially increases external memory addressing range in some cases. The LPC1788 is pin-compatible with the LPC2478 but contains a Cortex M3 processor core instead of an ARM7.

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

2,929 次查看
lpcware-support
Fresh Out Contributor

I think this is wrong.

According to the user manual UM10470, the 'address shift'
only applies to static ram, NOT to SDRAM (dynamic RAM).

0 项奖励
回复