After a software reset like WD reset, BOD reset, is the SRAM content retained?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

After a software reset like WD reset, BOD reset, is the SRAM content retained?

3,417件の閲覧回数
lpcware-support
Senior Contributor I

Yes. In case of a software reset like WD reset, BOD reset etc, the SRAM contents (memory address 0x1000 0000 to 0x1000 2000 in case of LPC1227 ) is retained. However, the part won't retain the contents if it goes to deep power-down mode or if the microcontrollers is unpowered.

0 件の賞賛
返信
1 返信

2,961件の閲覧回数
lpcware-support
Senior Contributor I

I test the LPC1225FBD48/321,after a WD reset all the SRAM data is 0,why?the address is 0x1000 0200, I test it in KEIL.
It is important to my program,after the WD reset, or soft reset the SRAM data should retain unchanged to keep the output steady.

0 件の賞賛
返信