void FLEXCAN_DRV_IRQHandler (uint8_t instance)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

void FLEXCAN_DRV_IRQHandler (uint8_t instance)

1,688 次查看
Anonymous
不适用

Hi Everyone,

 

I wants to use CAN interrupt . Is there any example code for this? I am using FRDM64 Board.

 

Kinetis SDK v.1.3 API Reference Manual.pdf don't have much information about it.

 

Thanks in advance.

 

Regards

Rishi

标签 (1)
0 项奖励
回复
1 回复

1,454 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Rishi,

please take a look at example for FlexCAN, the project is located under

<SDK_Install>/examples/<board>/driver_examples/flexcan/<use-case>/<toolchain>

there are two examples - FlexCAN Loopback and FlexCAN Network and because these examples are done for TWR-K64F120M, TWR-K60D100M, TWR-K65F180M, TWR-K21F120M and TWR-KV11Z75M, is needed to do some modifications for your board.

In case of FRDM-K64F, please connect TJA1050 according to TWR-SER Schematic to PTB18 and PTB19 and it should works.

TJA1050.png

schematic.png

More description for each flexcan functions you can get in fsl_flexcan_driver.h, located under C:\Freescale\KSDK_1.3.0\platform\drivers\inc

void FLEXCAN_DRV_IRQHandler(uint8_t instance);

/*!

* @brief Returns whether the previous FLEXCAN transmit has finished.

*

* When performing an async transmit, call this function to ascertain the state of the

* current transmission: in progress (or busy) or complete (success).

*

* @param instance The FLEXCAN module base address.

* @return The transmit status.

* @retval kStatus_FLEXCAN_Success The transmit has completed successfully.

* @retval kStatus_FLEXCAN_TxBusy The transmit is still in progress.

*/

I hope this helps.

Best Regards,

Iva

0 项奖励
回复