printf() with float values

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

printf() with float values

ソリューションへジャンプ
15,658件の閲覧回数
matthias
Contributor III

Hello,

 

I am using KSDK 1.1.0 with MQX and Processor Expert. Using printf() usually works fine, but I cannot make printf to print float/double values. For the code

 

float val = 1.234;

printf("Value = %f unit\n", val);


the output is

 

Value = f


I guess the reason is because printf() does not support float with the default KSDK settings for MQX, so I added  "#define MQX_INCLUDE_FLOATING_POINT_IO 1" to mqx_sdk_config.h but the behavior is still the same.

Any hints what I am doing wrong?

 

Regards

Matthias

ラベル(1)
1 解決策
11,845件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Matthias,

I have reproduced your finding and have submitted a trouble ticket to our MQX KSDK team.

Documentation should be updated and we should have a master location to define the STD_FP_IO option/capability.

My workaround...

Change std_prv.h to following:

#ifndef STD_FP_IO//DES added #ifndef
#define STD_FP_IO 0

#endif

And in the project Properties...add Defined for "STD_FP_IO=1":

ScreenHunter_111 Feb. 17 11.17.gif

Regards,

David

元の投稿で解決策を見る

10 返答(返信)
11,845件の閲覧回数
rajbatra
Contributor IV

I just tried this - went to mqx_stdlib_Source/include/std_prv.h and set "#define STD_FP_IO 1"  (I'll do the ifndef once this works).

I recompiled the KSDK libraries: mqx_stdlib_frdmk64f, ksdk_mqx_lib, ksdk_platform_lib_K64F12, and mqx_frdmk64f  and did a simple printf w/ floating point.

I get MQX_UNHANDLED_INTERRUPT (0x0041) exception.

Setting it back to 0, printf works as expected.

What am I missing?

Thanks,

-Raj

0 件の賞賛
返信
11,845件の閲覧回数
rajbatra
Contributor IV

Silly mistake - I was getting a stack over flow because stack size was set too small for printf floating point support. Once I increased stack, floating point printing worked. FYI, the -u _printf_float made no difference, just Matthias/David's comment to define STD_FP_IO to 1.

Thanks,

-Raj

0 件の賞賛
返信
11,845件の閲覧回数
syedidris
Contributor III

Hi I am getting same float printing problem in kinetis design studio 3.0.0 how to solve this?

0 件の賞賛
返信
11,845件の閲覧回数
dorianhildebran
Contributor I

A easyer way is:

Under Project Settings -> C/C++ Build -> Settings -> Tool Settings -> Miscellaneous

enable the Checkbox: "Use float with nano printf".

0 件の賞賛
返信
11,845件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Matthias,

are you using KDS/GNU libraries? If so, have you added

-u _printf_float

to the linker options?

(see printf() and scanf() with GNU ARM Libraries | MCU on Eclipse).

I hope this helps,

Erich

0 件の賞賛
返信
11,845件の閲覧回数
matthias
Contributor III

Hello Erich,

thanks for the quick reply. I am using  the MQX libraries that are included in KSDK. I have seen your post on mcuoneclipse.com (which helped me many times before :-)) and I have tried -u _printf_float in the linker options without success (I guess this option does not apply for KSDK libraries). I think the problem lies somewhere in the configuration of the KSDK/MQX libraries.

Regards

Matthias

0 件の賞賛
返信
11,845件の閲覧回数
matthias
Contributor III

I found a soultion now, but I am not very comfortable with it yet:

In the KSDK source code, there is a file "std_prv.h" where STD_FP_IO is defined. Setting this define to "1", printf() works with float. But as said, I am not comfortable with changing a file in the KSDK source code.

0 件の賞賛
返信
11,846件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Matthias,

I have reproduced your finding and have submitted a trouble ticket to our MQX KSDK team.

Documentation should be updated and we should have a master location to define the STD_FP_IO option/capability.

My workaround...

Change std_prv.h to following:

#ifndef STD_FP_IO//DES added #ifndef
#define STD_FP_IO 0

#endif

And in the project Properties...add Defined for "STD_FP_IO=1":

ScreenHunter_111 Feb. 17 11.17.gif

Regards,

David

11,845件の閲覧回数
eyeow84
Contributor III

Hi David,

So is it applicable for CW 10.6 with MCU MKE06Z as well? I have posted similar question about printf(%f) at here https://community.nxp.com/thread/438758 

Thanks...

0 件の賞賛
返信
11,845件の閲覧回数
rogerchaplin
Contributor II

Just thought I'd add my $0.02 worth for anybody else in this situation. I'm using KSDK 1.2.0 with Processor Expert in KDS 3.0 to create code to be built with IAR Embedded Workbench. I've added the MQX component to my project and chosen the standard MQX instead of MQX Lite. I found that the right place to put the define for STD_FP_IO = 1 is in the Component Inspector for MQX, in the User settings Definitions dialog:

pastedImage_0.png

Also be sure to make the change to std_prv.h in the KDS project. If you change any of the generated files outside the Processor Expert environment (i.e. you edit them in IAR Workbench) you'll get errors from Processor Expert the next time you try to generate code.