non blocking printf on Kinetis/sdk 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

non blocking printf on Kinetis/sdk 2

1,479 Views
manfredeggersdo
Contributor I

Hello,

I am using a MKM34Z256 - with Kinetis Design Studio and SDK V2 enviroment and FreeRTOS.

If I use the PRINTF Function, it looks like this funktion use the "UART_WriteBlocking" Function and so it blockes the rest of the system while giving out the UART-Data.

 

In fsl_debug_console.c in row 244 (approx) is the command:

 

 s_debugConsole.ops.tx_union.UART_PutChar = UART_WriteBlocking;

 

How can I change this to use the non blocking transfer function?

Thank You!

With best Regards

Manfred

Labels (1)
0 Kudos
Reply
1 Reply

1,325 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Manfred,

As you see that there are two or three transfering mode:polling mode, interrupt mode and DMA mode, in the example based on Freertos, the printf() or putchar() use polling mode. if you use interrupt mode or DMA mode, it is complicated.

Considering the fact that there is not much information to output to UART, I think it is okay.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply