missing mandatory configuartion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

missing mandatory configuartion

Jump to solution
10,579 Views
prabhakaranvelu
Contributor II

Hi

I use TWR-K65MF180M ,When I try to debug hello world ,I get error/ saying Missing mandatory configuration.Fill-in the 'Config options.'field in the debugger tab.What shall be the config option

Labels (1)
1 Solution
9,311 Views
prabhakaranvelu
Contributor II

Hi Iva,

I 've used KDS IDE .

Issue is resolved if add -d kinetis.cfg in other options (Debug Configurations >Debugger > Other Options).

-Prabha

View solution in original post

6 Replies
9,311 Views
eslamessa
Contributor I

Hi

I use FRDM-KW40Z , and have the same problem however I add "-d kinetis.cfg" in other options (Debug Configurations >Debugger > Other Options) nothing is changed

Untitled.png

0 Kudos
Reply
9,311 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Prabhakaran Veluchamy​,

Please, what IDE do you use? Can you take a picture/print screen of the issue/your configurations and attach here?

Thank you.

Best Regards,

Iva

9,312 Views
prabhakaranvelu
Contributor II

Hi Iva,

I 've used KDS IDE .

Issue is resolved if add -d kinetis.cfg in other options (Debug Configurations >Debugger > Other Options).

-Prabha

9,311 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Prabhakaran,

ok, thank you.

In case of any issue, please let us know.

Best Regards,

Iva

0 Kudos
Reply
9,302 Views
prabhakaranvelu
Contributor II

Hi Iva,

I use TWR-K65F180M with Kinetis KDS IDE V3.0.

It works fine with OPEN SDA USB driver so that results are displayed in

UART IO TERMINAL.

I tried to use Semihosting feature (is it working for V3.0 KDS?) and if

enable same and compile I find the UART IO terminal is disabled (as

expected so that result shall be disabled in semihosting console in IDE)

but error window appear as enclosed and debug execution is stopped.

Regards,

Prabhakaran Veluchamy

Devices Engineering

Penang Design Center

  • Motorola Solutions (M) Sdn Bhd.(Innoplex),No. 2A, Medan Bayan Lepas,Mukim

12, S.W.D.11900 Bayan Lepas,Penang*

motorolasolutions.com <http://www.motorolasolutions.com/>

  • Off: +6*04-2527864

E: [email protected]

On Fri, Mar 11, 2016 at 5:31 PM, ivadorazinova <

0 Kudos
Reply
9,302 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Prabhakaran,

Please refer to this article Semihosting for Kinetis Design Studio V3.0.0 and GNU ARM Embedded (launchpad) | MCU on Eclipse

I hope this helps you.

Best Regards,

Iva

0 Kudos
Reply