ksdk 1.3 usb stack compile errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ksdk 1.3 usb stack compile errors

1,385 Views
michaelhuslig
Contributor IV

After modifying an MSD device project from the 1.3 examples, I started getting compile errors when using the bare metal usb stack.  The errors pointed to the "#define _CODE_PTR_ *" line in types.h.  After much searching, I figured out that "usb_device_stack_interface.h" must be included before "usb_class.h".  On the next iteration of the stack, you might want to add that to usb_class.h.

 

Mike

Labels (1)
1 Reply

1,214 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mike,

Thanks for letting us know about it! I will report it to the ksdk team.

BTW, KSDK 2.0 is available now, maybe you can try it. Please kindly refer to Welcome to Kinetis Expert | Kinetis Expert for details.


Have a great day,
Kan

NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply