is there some example using freemaster+frdm-k64f + PE+kds3.0+ sdk 1.2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is there some example using freemaster+frdm-k64f + PE+kds3.0+ sdk 1.2?

ソリューションへジャンプ
5,488件の閲覧回数
jordangarcia
Contributor II

Hey guys, I'm an engineering student and I´d like to use freemaster componet in the new kds and sdk versions (3.0 and 1.2)  to watch my global variables (like codewarrior does) and watch them in a graphic mode.

 

Could you provide me an example using frdm-k64+pe+sdk ? Please

 

Thanks.

ラベル(1)
1 解決策
4,799件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jordan,

attached is an example I'm using in one of my courses.

I plan to write a tutorial about it,but have not finished it yet.

I hope this helps,

Erich

元の投稿で解決策を見る

4 返答(返信)
4,800件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jordan,

attached is an example I'm using in one of my courses.

I plan to write a tutorial about it,but have not finished it yet.

I hope this helps,

Erich

4,798件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Attached is a hands-on slide deck for a hands-on workshop which shows using Kinetis Design Studio v3.0.0, Kinetis SDK v1.2, FreeMASTER v1.4 with the FRDM-K64F board.

I hope this this is useful.

Erich

4,798件の閲覧回数
rogerchaplin
Contributor II

This slide deck is excellent. Your instructions are very clear, and I was able to use them to get FreeMASTER up and running on a TWR-KV31F512 board even though you wrote the tutorial for a different board. Well done!

0 件の賞賛
返信
4,798件の閲覧回数
jordangarcia
Contributor II

Thanks Erich :

The information is great (like always) and the example too. :smileywink:

Regards.

Jordan.

0 件の賞賛
返信