httpserver_freertos Demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

httpserver_freertos Demo

ソリューションへジャンプ
1,339件の閲覧回数
kooroshhajiani
Contributor III

Hi,

I'm running the following demo:

C:\Freescale\KSDK_1.3.\examples\twrk64f120m\demo_apps\lwip\lwip_httpserver_demo\httpserver_rtos\httpserver_freertos\kds

It works as far as TCP/IP however I don't have serial communication via DB9.

I'm using TWR_K64F120 + TWR_SER2 board. I have run several project and demo with this set up and I've had serial communication VIA the DB9 as long as I configured UART5 for the printf port but this one is not budging.

Any Ideas?

 

Thanks,

Koorosh Hajiani

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,241件の閲覧回数
kooroshhajiani
Contributor III

I had to enable the CLK for port E.

Sorry for the waste of time.

Thanks,

KH

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,242件の閲覧回数
kooroshhajiani
Contributor III

I had to enable the CLK for port E.

Sorry for the waste of time.

Thanks,

KH

0 件の賞賛
返信