When will KSDK support be available for the MK22FN1M0VLK12?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When will KSDK support be available for the MK22FN1M0VLK12?

Jump to solution
3,187 Views
jeffreygraves
Contributor III

When will KSDK support be available for the MK22FN1M0VLK12?

 

When will the next KSDK update be available?

 

The MK22FN1M0VLK12 is an 80 pin part.

If I configure my project (KDS_2.0 and KSDK_1.1.0) for a MK22FN512CAP12 (80pin BGA), would it run on the MK22FN1M0VLK12 (80pin LQFP)?

 

(We don't yet need USB...)

 

Does anyone have experience running KSDK_1.1.0 based code on a MK22FN1M0VLK12?

 

Thank you,

Labels (1)
Tags (3)
1 Solution
2,836 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Jeffrey Graves,

supposed term is for KSDK 1.2 is end of April.

If anything changes, I'll let you know.


Best Regards,

Iva

View solution in original post

0 Kudos
Reply
4 Replies
2,836 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Jeffrey Graves,

the configured project for MK22FN512CAP12 will run on the MK22FN1M0VLK12,

but you should set the parametres in boards.h, specifically pin_mux.c.


If you do these points, project will run.


Best Regards,

Iva

2,836 Views
jeffreygraves
Contributor III

Thank you Iva.

Do you know when the next KSDK update will be available?

0 Kudos
Reply
2,836 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jeffrey Graves:

Good news! There is now a standalone version of KSDK for TWR-K21F120M. This board has a K21FN1M0, which is practically identical to K22FN1M0.

You can get it from the "Downloads" tab in the product page:

Kinetis K21 120 MHz Tower System Module|Freescale

Regards!

Jorge Gonzalez

2,837 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Jeffrey Graves,

supposed term is for KSDK 1.2 is end of April.

If anything changes, I'll let you know.


Best Regards,

Iva

0 Kudos
Reply