When will KSDK support be available for the MK22FN1M0VLK12?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

When will KSDK support be available for the MK22FN1M0VLK12?

跳至解决方案
3,148 次查看
jeffreygraves
Contributor III

When will KSDK support be available for the MK22FN1M0VLK12?

 

When will the next KSDK update be available?

 

The MK22FN1M0VLK12 is an 80 pin part.

If I configure my project (KDS_2.0 and KSDK_1.1.0) for a MK22FN512CAP12 (80pin BGA), would it run on the MK22FN1M0VLK12 (80pin LQFP)?

 

(We don't yet need USB...)

 

Does anyone have experience running KSDK_1.1.0 based code on a MK22FN1M0VLK12?

 

Thank you,

标签 (1)
标记 (3)
1 解答
2,797 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Jeffrey Graves,

supposed term is for KSDK 1.2 is end of April.

If anything changes, I'll let you know.


Best Regards,

Iva

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,797 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Jeffrey Graves,

the configured project for MK22FN512CAP12 will run on the MK22FN1M0VLK12,

but you should set the parametres in boards.h, specifically pin_mux.c.


If you do these points, project will run.


Best Regards,

Iva

2,797 次查看
jeffreygraves
Contributor III

Thank you Iva.

Do you know when the next KSDK update will be available?

0 项奖励
回复
2,797 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jeffrey Graves:

Good news! There is now a standalone version of KSDK for TWR-K21F120M. This board has a K21FN1M0, which is practically identical to K22FN1M0.

You can get it from the "Downloads" tab in the product page:

Kinetis K21 120 MHz Tower System Module|Freescale

Regards!

Jorge Gonzalez

2,798 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Jeffrey Graves,

supposed term is for KSDK 1.2 is end of April.

If anything changes, I'll let you know.


Best Regards,

Iva

0 项奖励
回复