What's the issue with libsdk_platform.a ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What's the issue with libsdk_platform.a ?

792 次查看
garytivey
Contributor I

Recent install of latest Kinetics SDK, and I can't get "hello_world" to compile...

Have followed the instructions in the somewhat sketchy PDF for Linux installs... seems to be pretty buggy and the doc's are mostly for windowz platform.

I have used Kinetics on Linux (Fedora) over the past 2-3 years, so I'm at a loss to get this going. The freakin' ARM tool-chain is always a moving target.:-)

 

Thanks in advance,

Gary

标签 (1)
0 项奖励
回复
1 回复

692 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Gary Tivey

SDK 2.x doesn't need to compile platform library, If you have to compile libsdk_platform.a you probably have SDK 1.x version.

If you want to update to the latest version of SDK you can download it here; Welcome to MCUXpresso | MCUXpresso Config Tools , if you are using KDS, Also, you will need Service Pack: Eclipse add-on to add Kinetis SDK V2.x Project Wizard v2.0.1, You can find it in the KDS download page.

If you want to use the version that you have, you need to first compile libsdk_platform.a library, it is located in the path: <KSDK_path>\lib\ksdk_platform_lib\<your_IDE>\<your_device>

Hope this information could help you

Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复