What changes needed to support MK22FN1M0VLH12 MCU for KSDK V-1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What changes needed to support MK22FN1M0VLH12 MCU for KSDK V-1.2

Jump to solution
1,448 Views
sureshkumawat
Contributor I

Hi,

I have my driver which is already ported for MK22FN1M0VLH12 MCU for MQX-4.2. I want it to port for KSDK v1.2 with KDS 3.0 . I have referred Kinetis SDK v.1.2.0 Release documents, Here in this document in supported MCU list i am not finding my MCU name so i am in doubt that KSDK supports this MCU or not. Have anyone idea that KSDK supports MK22FN1M0VLH12 MCU or not.

 

Or Is there any alternate way to get support of KSDK for my MCU?

Regards,

Suresh

Labels (1)
0 Kudos
Reply
1 Solution
1,289 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Suresh,

As so far , the KSDK1.2 doesn't support this chip  MK22FN1M0VLH12 ,

you can see on the website about h the information :

K22_120 |Kinetis K22 120 MHz MCUs|Freescale

pastedImage_1.png

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,289 Views
ivadorazinova
NXP Employee
NXP Employee

Hello suresh kumawat,

at the moment MK22FN1M0VLH12 is not supported by current KSDK.

But you can port it by yourself according to this document.

I hope this helps.

Best Regards,

Iva

0 Kudos
Reply
1,290 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Suresh,

As so far , the KSDK1.2 doesn't support this chip  MK22FN1M0VLH12 ,

you can see on the website about h the information :

K22_120 |Kinetis K22 120 MHz MCUs|Freescale

pastedImage_1.png

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------