What changes needed to support MK22FN1M0VLH12 MCU for KSDK V-1.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What changes needed to support MK22FN1M0VLH12 MCU for KSDK V-1.2

ソリューションへジャンプ
2,331件の閲覧回数
sureshkumawat
Contributor I

Hi,

I have my driver which is already ported for MK22FN1M0VLH12 MCU for MQX-4.2. I want it to port for KSDK v1.2 with KDS 3.0 . I have referred Kinetis SDK v.1.2.0 Release documents, Here in this document in supported MCU list i am not finding my MCU name so i am in doubt that KSDK supports this MCU or not. Have anyone idea that KSDK supports MK22FN1M0VLH12 MCU or not.

 

Or Is there any alternate way to get support of KSDK for my MCU?

Regards,

Suresh

ラベル(1)
0 件の賞賛
返信
1 解決策
2,172件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Suresh,

As so far , the KSDK1.2 doesn't support this chip  MK22FN1M0VLH12 ,

you can see on the website about h the information :

K22_120 |Kinetis K22 120 MHz MCUs|Freescale

pastedImage_1.png

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,172件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello suresh kumawat,

at the moment MK22FN1M0VLH12 is not supported by current KSDK.

But you can port it by yourself according to this document.

I hope this helps.

Best Regards,

Iva

0 件の賞賛
返信
2,173件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Suresh,

As so far , the KSDK1.2 doesn't support this chip  MK22FN1M0VLH12 ,

you can see on the website about h the information :

K22_120 |Kinetis K22 120 MHz MCUs|Freescale

pastedImage_1.png

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------