Watchdog example SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog example SDK

4,926件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I used the example for the watchdog coming with the SDK. I am not using the frdm board, it should not be a problem, the

code is just basic. I am not able to refresh the watchdog, once started it will ineluctably reset the processor after the set time.

The set timeout is correct but no way to reset the count.

I use the K64 processor..

Is there a suggestion???

 

Thank You all

Pietro

ラベル(1)
タグ(1)
8 返答(返信)

4,138件の閲覧回数
pietrodicastri
Senior Contributor II

I have installed the 1.2 but my existing works are still using the 1.1. So I am experimenting with this version, since I have seen the backward compatibility is not provided. I have further tried, I see if I clean, close, delete the project(without delete) , than import again, the projects compile again. Something is not in order anyway, but the situation begins to be lighter.

One thing I would like to understand is the nanolib option. The only way to -build the projects is to use the  specs=nano.specs -specs=nosys.specs

while the nanolib is producing errors. If You provide me a better explanation of this it is of help. I will try to process the original question, if the watchddow example works.

Thank You for support

0 件の賞賛
返信

4,138件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

if you port projects from KDS 2.0 to KDS 3.0 there are more parameters, you should change (flags for processor and options for linker).

Please, see the tutorial

Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V...

I hope this helps you,

Iva

4,138件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Pietro,

Are you using the latest KDS_3.0 and KSDK_1.2.0?

For issues like this best to post your project as well.

Regards,

David

0 件の賞賛
返信

4,138件の閲覧回数
pietrodicastri
Senior Contributor II

I am using the KDS 2.0 and the SDK 1.1.0...

Thank You

0 件の賞賛
返信

4,138件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Pietro,

Can you try upgrading and re-testing?

Regards,

David

4,138件の閲覧回数
pietrodicastri
Senior Contributor II

Hei David

I tried to install the KDS 3. Nothing works.

In the 2.0 version importing a project automatically imports the SDK if not already in the workspace. Here it does not happen.

I imported the SDK manually and it is impossible to build. The error is

arm-none-eabi-gcc: fatal error: no input files

I have now a useless setup.. I need a quick support, or it is better for me to scrap this update..

Thank You

Pietro

0 件の賞賛
返信

4,138件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

and have you already installed KSDK 1.2 ?

What do you use for the operating system?

Please, did you follow these steps?

Video Link : 3281

Best Regards,

Iva

4,138件の閲覧回数
pietrodicastri
Senior Contributor II

Hi David

When possible, now I am in the hell of delivering to customer. I will survive with what I have

You will know

Thank You

0 件の賞賛
返信