Watchdog driver KSDK2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog driver KSDK2.0

1,312件の閲覧回数
manfredschnell
Contributor IV

Hi,

 

we use KSDK2.0 with K64.

 

In "Kinetis SDK v.2.0 API Reference Manual"  Document Number: KSDK20APIRM, Rev. 0.

I found COP_Init(), and COP_xxxx () functions to use the internal Watchdog unit.

 

In KSDK2.0 source "fsl_wdog.c" I found:

WDOG_Init(), and WDOG_xxx () functions, that seems to use the internal Watchdog unit of my K64.

 

Am I wrong? Is there a difference?

I think there is a naming discrepancy from source to Reference Manual.

 

Best regards

Manfred

ラベル(1)
0 件の賞賛
返信
1 返信

1,111件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Manfred,

Short answer they are different.

Longer answer.  The COP is a module for the Kinetis L MCU's and WDOG is module for the Kinetis K MCU's.  I think the Reference Manuals (I looked at K64 and KL25 as examples) indicate this best but could use a little cleanup.  The KSDK_v2.0 API Reference Manual needs additional verbage to indicate if the API applies to the specific MCU or not or the API should only have the API's that apply to the specific MCU.

I'll forward to our KSDK team.

Regards,

David

0 件の賞賛
返信