USBDM 4.6.10.250a Install problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM 4.6.10.250a Install problem

1,733件の閲覧回数
GeorgeChamberla
Contributor I

I have installed:-

USBDM_4_10_6_250a_Win  and  USBDM_Drivers_1_3_0_Win_x64  on Windows 7

 

Using 'ARM GDB Server' setup I can detect the MKE04Z804 processor OK  on my FRDM-KE04Z Dev PCB

 

But I get the following error on exit:-

Welcome to USBDM GDB server

ERROR: Could not create server at the specified port !

 

Please Help

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,539件の閲覧回数
pgo
Senior Contributor V

Hi George,

The only time I have seen this error is when there is already a program using that port.

I assume you are experimenting with the stand-alone server launched from the Windows Start Menu.  Can you try changing the server port if you have not already tried this.

pastedImage_0.png

The only other suggestion is related to networking and firewalls.  Is it possible that the GDB server is not allowed to create sockets?

bye

0 件の賞賛
返信

1,539件の閲覧回数
GeorgeChamberla
Contributor I

Thanks for the reply.

Changing the GDB Server Port number fixed it.  Thank you.

0 件の賞賛
返信