USB stack composite device 6 cdc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB stack composite device 6 cdc

2,393 Views
andoniiba1
Contributor II


I am using a TWR - K65F180M board. I amtrying to implement a usb composite device with 6 cdc usuing the usb stack included in the KSDK 1.3.0. I was able to configure the stack to use 5 CDC but when I add the 6th the PC does not enumerate any of the COMs. Can some one help me?

Labels (1)
Tags (1)
3 Replies

2,286 Views
isaacavila
NXP Employee
NXP Employee

Hello Andoni,

Every CDC interface does use 3 endpoints (One IN Interrupt endpoint, One IN Bulk Endpoint and One OUT Bulk Endpoint, 3 in Total) each, so, if you are using 3 different endpoints for every interface, then you have used 15 endpoints for first 5 CDCs. Once you want to add a new one, then you do not have enough endpoints for next CDC interface.

So you are probably using all available endpoints. Could you please confirm this?

I hope this can help you!

Best Regards,

Isaac

2,286 Views
andoniiba1
Contributor II

Hello Isaac,

You are correct I am using 3 endpoints per CDC, but I modified the following macros:

#define KHCI_MAX_ENDPOINT 19  (originally 16)

#define USBCFG_DEV_MAX_ENDPOINTS  19   (originally 16)

#define MAX_DEVICE_SERVICE_NUMBER     19    (originally 16)

Is there a limitation of 16 endpoints in the usb stack?

Best Regards,

Andoni

0 Kudos
Reply

2,286 Views
isaacavila
NXP Employee
NXP Employee

Hello Andoni,

You cannot use more than 16 endpoints, USB uses only 16 endpoints (bidirectional) so you cannot extend this value to a higher value. You will need to use the bidirectional feature (use for example, endpoint 1 OUT and endpoint 1 IN for one CDC device) for each endpoint in order to have enough endpoints for all 6 CDC devices:

Endpoints.jpg

I hope this helps!

Regards,

Isaac