USB Composite MSD, CDC device with Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Composite MSD, CDC device with Processor Expert

1,572 次查看
AlexJLennon
Contributor III

Hi,

 

I'm using KDS and KSDK 1.3.0 to build a project supporting USB composite for an MSD device and a CDC device. This is with a K22 series part.

 

However I've run into problems.

 

I have the MSD device working, but I am using MQX Full and there seems to be an incompatibility which prevents me from enabling serial debug console support.

 

I had hoped to see an fsl_usb_device_cdc_class component which would provide what I need but this doesn't seem to be present.

 

It's looking like I might have to lose Processor Expert support for USB and work around this, which would be a shame.

 

Can anybody offer advice?

 

Thanks,

 

Alex Lennon

标签 (1)
0 项奖励
回复
1 回复

1,248 次查看
isaacavila
NXP Employee
NXP Employee

Hello Alex,

Could you please share your project in order to check what modifications need to be done in order to enable serial debug console?

Thanks,

Isaac

0 项奖励
回复