USB Composite MSD, CDC device with Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Composite MSD, CDC device with Processor Expert

1,568件の閲覧回数
AlexJLennon
Contributor III

Hi,

 

I'm using KDS and KSDK 1.3.0 to build a project supporting USB composite for an MSD device and a CDC device. This is with a K22 series part.

 

However I've run into problems.

 

I have the MSD device working, but I am using MQX Full and there seems to be an incompatibility which prevents me from enabling serial debug console support.

 

I had hoped to see an fsl_usb_device_cdc_class component which would provide what I need but this doesn't seem to be present.

 

It's looking like I might have to lose Processor Expert support for USB and work around this, which would be a shame.

 

Can anybody offer advice?

 

Thanks,

 

Alex Lennon

ラベル(1)
0 件の賞賛
返信
1 返信

1,244件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Alex,

Could you please share your project in order to check what modifications need to be done in order to enable serial debug console?

Thanks,

Isaac

0 件の賞賛
返信