USB Composite MSD, CDC device with Processor Expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Composite MSD, CDC device with Processor Expert

1,644 Views
AlexJLennon
Contributor III

Hi,

 

I'm using KDS and KSDK 1.3.0 to build a project supporting USB composite for an MSD device and a CDC device. This is with a K22 series part.

 

However I've run into problems.

 

I have the MSD device working, but I am using MQX Full and there seems to be an incompatibility which prevents me from enabling serial debug console support.

 

I had hoped to see an fsl_usb_device_cdc_class component which would provide what I need but this doesn't seem to be present.

 

It's looking like I might have to lose Processor Expert support for USB and work around this, which would be a shame.

 

Can anybody offer advice?

 

Thanks,

 

Alex Lennon

Labels (1)
0 Kudos
Reply
1 Reply

1,320 Views
isaacavila
NXP Employee
NXP Employee

Hello Alex,

Could you please share your project in order to check what modifications need to be done in order to enable serial debug console?

Thanks,

Isaac

0 Kudos
Reply