UART3_RX_TX_IRQHandler missing first byte in isr

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART3_RX_TX_IRQHandler missing first byte in isr

1,862件の閲覧回数
Anonymous
適用対象外

Dear All,

I have problem in receiving bytes in ISR see below code.

 

void UART3_RX_TX_IRQHandler(void)

{

    UART_DRV_IRQHandler(3);

    if(inx>9)

    {

               inx=0;

 

    }

    UART_HAL_Getchar(UART3, &RxBuff[inx]);

    inx++;

}

I am sending 8 bytes (1,2,3,4,5,6,7,8) but first  receiving  is wrong RxBuff[0] =0xFF instead of 1 remaining 7 bytes are good.

 

MY TX & RX pins are short.

 

My suspect is RX interrupt is not enabled.

 

Thanks in advance

 

Regards

rishi

ラベル(1)
2 返答(返信)

1,586件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Rishi Kumar:

There is no need to call the API UART_HAL_Getchar(). This is already done inside of UART_DRV_IRQHandler() and the Rx Buffer should be automatically filled with the received bytes, you only need to call the driver APIs UART_DRV_ReceiveData() or UART_DRV_ReceiveDataBlocking(). See the attached example I made for a FRDM-K64F. If you are using a different board just adjust the clock gate, uart instance and pins as required.

:smileyinfo: NOTE: This main.c assumes that the file fsl_uart_irq.c is already part of the project.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,586件の閲覧回数
Anonymous
適用対象外

Dear Mr. Jorge ,

Thanks for support. It is working fine but In my case i don't know the receiving packet length.

So that I can read complete packet without losing bytes or mixing with next packet.

How i can check the SCI Idle status Flag in K64F? I need example for this too.

Thanks & regards

Rishi

0 件の賞賛
返信