UART 7816 with K32L2B1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART 7816 with K32L2B1

ソリューションへジャンプ
3,459件の閲覧回数
cate
Contributor I

I'm using the K32L2B1 mcu and I need to use the UART in 7816 mode. However, I could not find in the SDK the drivers that set the UART in that mode. 

Am I missing some file or I have to implement the drivers myself?

0 件の賞賛
返信
1 解決策
3,443件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, we do not have specific drivers that implement smart card interface. However, reference manual provides in detail how to program the UART for ISO-7816 operation. Please refer to section 38.9.1.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"  button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,444件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, we do not have specific drivers that implement smart card interface. However, reference manual provides in detail how to program the UART for ISO-7816 operation. Please refer to section 38.9.1.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"  button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 件の賞賛
返信