The LPSCI question of KL36

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The LPSCI question of KL36

1,252 次查看
小勇邹
Contributor II

Hi,

 

I am using the LPSCI of KL36.I use the example ...\examples\frdmkl46z\driver_examples\lpsci\lpsci_blocking.

 

1) The SCI is OK when configuring SCI as fellow shown.The data that is sent to the software in my computer is correct. 

    lpsci_user_config_t lpsciConfig = {
#if defined(KL02Z4_SERIES)
        .clockSource     = kClockLpsciSrcFll,
#else
        .clockSource     = kClockLpsciSrcPllFllSel,
#endif
        .bitCountPerChar = kLpsci8BitsPerChar,
        .parityMode      = kLpsciParityDisabled,
        .stopBitCount    = kLpsciOneStopBit,
        .baudRate        = BOARD_DEBUG_UART_BAUD
    };

 

2) But it is not OK when I change  ".parityMode      = kLpsciParityDisabled," to ".parityMode      =kLpsciParityEven".

The data that is sent to the software in my computer is not correct. The software  in my computer is also configured as "ParityEven".

标签 (1)
0 项奖励
回复
1 回复

1,149 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Robin,

     Please bitCountPerChar  to kLpsci9BitsPerChar, the configuration code should like this:

    // Fill in lpsci config data
    lpsci_user_config_t lpsciConfig = {
#if defined(KL02Z4_SERIES)
        .clockSource     = kClockLpsciSrcFll,
#else
        .clockSource     = kClockLpsciSrcPllFllSel,
#endif
        .bitCountPerChar = kLpsci9BitsPerChar,//kLpsci8BitsPerChar,
        .parityMode      = kLpsciParityEven,//kLpsciParityDisabled,
        .stopBitCount    = kLpsciOneStopBit,
        .baudRate        = BOARD_DEBUG_UART_BAUD
    };
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

      Then test it again, your PC will receive the correct data.

     Reason: if you enable the parity mode, and still select 8-bit Mode, because the parity still one bit, then the data in the uart wave will be 7 bit data+1 bit parity.

    Anyway, when you want to use the parity mode, please select 9 bits mode.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复