State Machine Working in MED-BPM Kinetics TWR-K53N512 in IAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

State Machine Working in MED-BPM Kinetics TWR-K53N512 in IAR

1,964 次查看
communitycommun
Contributor III

It would very helpful if someone who would tell me how the state machine (State idle,state measure,state abort) gets changed while the code is been flashed.


As far as reading the PDF for med bpm i have understood that after providing the input from GUI it changes the state,else it remain in the state idle mode.

 

Hope someone would have worked on this before...

 

Thanks ..

标签 (1)
2 回复数

1,777 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello,

I apologize for the late response, but I was out of office.

Please, take a look at this Application Note, Freescale Solutions for Electrocardiograph and Heart Rate Monitor Applications​  with the related sw http://cache.nxp.com/files/analog/doc/app_note/AN4323SW.zip

I hope this helps.

Best Regards,

Iva

1,777 次查看
communitycommun
Contributor III

Thanks Iva dorazinov,

                            I apologize for late response.

I had this document before .now i have understood the code and state machine....
Thanks for the reply....