State Machine Working in MED-BPM Kinetics TWR-K53N512 in IAR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

State Machine Working in MED-BPM Kinetics TWR-K53N512 in IAR

1,968件の閲覧回数
communitycommun
Contributor III

It would very helpful if someone who would tell me how the state machine (State idle,state measure,state abort) gets changed while the code is been flashed.


As far as reading the PDF for med bpm i have understood that after providing the input from GUI it changes the state,else it remain in the state idle mode.

 

Hope someone would have worked on this before...

 

Thanks ..

ラベル(1)
2 返答(返信)

1,781件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello,

I apologize for the late response, but I was out of office.

Please, take a look at this Application Note, Freescale Solutions for Electrocardiograph and Heart Rate Monitor Applications​  with the related sw http://cache.nxp.com/files/analog/doc/app_note/AN4323SW.zip

I hope this helps.

Best Regards,

Iva

1,781件の閲覧回数
communitycommun
Contributor III

Thanks Iva dorazinov,

                            I apologize for late response.

I had this document before .now i have understood the code and state machine....
Thanks for the reply....