Setting FBI mode with SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting FBI mode with SDK

Jump to solution
4,144 Views
pietrodicastri
Senior Contributor II

Good morning

I try to execute this call with different values of fcrdivVal, the fourth parameters in the function.

 

    CLOCK_HAL_SetFbiMode(MCG_BASE, kMcgDcoRangeSelMid, kMcgInternalRefClkSelFast, 5, CLOCK_FllStableDelay, &outClkFreq );

 

It execute correctly with values from 0 to 5. The clock is 125 KHz with a value of 5.

If the fcrdivVal is 6 the clock is updated (32KHz), I see on the scope as CLOCKOUT, but the debugger looses the control.

Is it normal???

Solutions???

 

Thank You

Labels (1)
Tags (3)
1 Solution
3,922 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Pietro,

Why do you change the divider when you use the FBI?

If you go to Reference Manual, page 593

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/K64P144M120SF5RM.pdf

reference manual.png

so, the value for fcrdivVal = 6, output frequency cannot be 32KHz.

Because when the value is 5, 4MHz and Divide Factor is 32, is 125KHz. It is right.

BUT: when is the value 6, 4MHz and Divide Factor is 64, it is 62,5KHz, not 32KHz.

(4MHz : 64 = 62,5KHz)


As it is written in the Reference Manual : you have not change the divider when the Fast IRC is enabled. 


Please, look to SIM Module, Register SIM_CLKDIV1->OUTDIV4 what is your frequency divider for flash memory.


Best Regards,

Iva



View solution in original post

7 Replies
3,922 Views
pietrodicastri
Senior Contributor II

Hi ..

I am still interested in some assistance.

Thank You

Pietro

0 Kudos
Reply
3,923 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Pietro,

Why do you change the divider when you use the FBI?

If you go to Reference Manual, page 593

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/K64P144M120SF5RM.pdf

reference manual.png

so, the value for fcrdivVal = 6, output frequency cannot be 32KHz.

Because when the value is 5, 4MHz and Divide Factor is 32, is 125KHz. It is right.

BUT: when is the value 6, 4MHz and Divide Factor is 64, it is 62,5KHz, not 32KHz.

(4MHz : 64 = 62,5KHz)


As it is written in the Reference Manual : you have not change the divider when the Fast IRC is enabled. 


Please, look to SIM Module, Register SIM_CLKDIV1->OUTDIV4 what is your frequency divider for flash memory.


Best Regards,

Iva



3,922 Views
pietrodicastri
Senior Contributor II

Hi Iva

Yes I should not divide in such condition. That's a good point.

Thank You

0 Kudos
Reply
3,922 Views
pietrodicastri
Senior Contributor II

Hi Iva

Sorry. I will detail..

KDS Version: 2.0.0

SDK 1.1.0

Thank You

0 Kudos
Reply
3,921 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pietro,

Can you tell me the part number of the Kinetis and the version of SDK?

BR

XiangJun Rong

3,922 Views
pietrodicastri
Senior Contributor II

Thank You for assistance

I am using the FRDM K64. I am debugging with the JTAG, in reduced version with only the two pins, as in the schematic.

I use the KDS.

I am suspicious the slow clock is not handled in this reduced JTAG connection...

Let me know

Best Regards

Pietro di Castri

0 Kudos
Reply
3,922 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Pietro,

like Rong said, we need exact information about versions, which you use.

KDS is IDE, Kinetis Design Studio and KSDK is Kinetis Software Development Kit.

You can find it on C:\Freescale and folders KDS_2.0.0 and KSDK_1.1.0.

Iva

0 Kudos
Reply