SPI Driver Not working Arm M0+ MKL15Z128VFT4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Driver Not working Arm M0+ MKL15Z128VFT4

1,237 Views
jonathan_guinta
Contributor I

I'm in the process of debugging a SPI peripheral I'm using with the ARM M0+ uC MKL15Z128VFT4. The OS is BareMetal and the SysTick is at 1ms. The clock speed for the SPI peripheral is 23.405714 kHz. I keep running into an issue where an exception is thrown when the hit the SPI_HAL_SetIntMode(base, kSpiRxFullAndModfInt) and then the debugger jumps to DefaultISR. I have the instruction set in Thumb mode and the debug level at Default -g. Also I do initialize the peripheral driver before this with:

 

//Install interrupt handler for SPI comm

    OSA_InstallIntHandler(SPI0_IRQn, SPI_COM1_IRQHandler);

    //Initialize SPI to Master control

    if(SPI_DRV_MasterInit(*m_instance, &SPI_COM1_MasterState) == kStatus_SPI_Success)

    {

//Configure the SPI bus
SPI_DRV_MasterConfigureBus(*m_instance, &SPI_COM1_MasterConfig0, &SPI_COM1_calculatedBaudRate);
return true;

    }

    return false;

 

So I can't imagine it's the proper initialization of the peripheral that's the cause of this exception being thrown, but I won't rule it out. Any pointers/ideas to help solve this would be much appreciated. BTW, if I manually step through the code with the debugger, the exception isn't thrown, since the debugger is controlling the execution. I've seen this issue arise in the past with the SysTick timer, or the debugger symbol file not being aligned. I'm not sure.

Labels (1)
0 Kudos
Reply
1 Reply

1,068 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jonathan,

Regarding your question, it seems that there is problem for the following function, pls check.

SPI_DRV_MasterInit(*m_instance, &SPI_COM1_MasterState);

SPI_DRV_MasterConfigureBus(*m_instance, &SPI_COM1_MasterConfig0, &SPI_COM1_calculatedBaudRate);

I do not know what you define the m_instance, if you define it as:

#define m_instance 1 //if you use SPI1

#define m_instance 0 //if you use SPI0

#define m_instance 2 //if you use SPI2

In the case, you should omit the * when you call the API function.

SPI_DRV_MasterInit(m_instance, &SPI_COM1_MasterState);

SPI_DRV_MasterConfigureBus(m_instance, &SPI_COM1_MasterConfig0, &SPI_COM1_calculatedBaudRate);

Hope it can help.

BR

Xiangjun Rong

0 Kudos
Reply