SPI DMA Clock spike

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI DMA Clock spike

1,633件の閲覧回数
nobodyKnows
Contributor III

Hello,

the disable of the SPI causing a high and the enable causing a low on the spi clock line.

 

status_t SPI_MasterTransferDMA(SPI_Type *base, spi_dma_handle_t *handle, spi_transfer_t *xfer) {

...

     /* Disable SPI and then enable it, this is used to clear S register*/

    SPI_Enable(base, false);

    SPI_Enable(base, true);

...

}

 

My spi slave recognise this a one clock cycle. I think this is a bug in KSDK2.0.

 

Best regards

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,505件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Maximilian,

Regarding your question, can you tell me the part number you are using? as you know that there are two IP for SPI, one is used in Kl family, called SPI. Another is used in K family, called dspi. I suppose you use spi implemented for example in KL family.

This is the spi_enable() function:

static inline void SPI_Enable(I2C_Type *base, bool enable)

{

    if (enable)

    {

        base->C1 |= SPI_C1_SPE_MASK;

    }

    else

    {

        base->C1 &= ~SPI_C1_SPE_MASK;

    }

}

Setting the SPE bit in SPIx_C1 register "enables the SPI system and dedicates the SPI port pins to SPI system functions", it is possible that the SCK pin logic toggles after setting the SPE. But the CS pin is invalid when the SCK toggles after setting SPE bit, I do not think it can take effect on the SPI slave side.

In conclusion, from slave side, using a CS pin to enable slave spi instead of connecting the CS pin to GND in slave spi side, the CS pin is driven by master.

Hope it can help you.

BR

Xiangjun Rng

0 件の賞賛
返信

1,505件の閲覧回数
nobodyKnows
Contributor III

Hello,

I use a KL26. I have more than one device so I use several GPIOs for chip select. So this is really a Problem.

Best Regards,

Maximilian

0 件の賞賛
返信