SDK support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK support

Jump to solution
4,483 Views
pietrodicastri
Senior Contributor II

Good morning

I have problem in identifying the support of the SDK for the following processors:

 

MK10DN32VMP5

MK10DX32VMP5

MK10DN64VMP5

MK10DX64VMP5

MK10DN128VMP5

MK10DX128VMP5

 

Are any of supported???

 

Thank You

 

 

Pietro

Labels (1)
0 Kudos
Reply
1 Solution
4,290 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

thank you for this very good question.

I checked your mentioned MCU and SDK support MCU and there is a main difference - there are different processors,

so there is no direct SDK support, but - I see support of KDS, so you can modify the code for KSDK.

I attach you the guide.

mk10.png

Does it help you?

Iva

View solution in original post

4 Replies
4,291 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

thank you for this very good question.

I checked your mentioned MCU and SDK support MCU and there is a main difference - there are different processors,

so there is no direct SDK support, but - I see support of KDS, so you can modify the code for KSDK.

I attach you the guide.

mk10.png

Does it help you?

Iva

4,290 Views
EarlOrlando
Senior Contributor II

Dear Pietro,

I am afraid that there is only support for the Kinetis K10 that runs at 100 MHz (MK10DNxxxxxx10 and MK10DXxxxxxx10).

Regards,

Earl.

/* If this post answers your question please click the Correct Answer button. */

0 Kudos
Reply
4,290 Views
joetrovato
Contributor I

Similarly,

Is the Kinetis K70 at 120Mhz supported by the KSDK?

Thank you!

0 Kudos
Reply
4,290 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Joe,

TWR-K70F120M will be supported in KSDK 1.3.

we expect it in Q3.

Best Regards,

Iva

0 Kudos
Reply