Registration Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Registration Code

2,920件の閲覧回数
JayJay
Contributor I

Hi

 

I have got a FRDM-K82F eval board, when I try to download the SDK I am being asked for a Registration Code, where do I get this code from?

 

Regards

Jay

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,884件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello,

For addition: whole procedure is described here

How to: install KSDK 2.0

Do you wait for an approval?

Thank you for your feedback.
Iva

0 件の賞賛
返信

1,884件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Jameel

The latest SDK version is v2.0, please click into the link below, and click on ‘Build an SDK’ to choose the board you are using:

Welcome to Kinetis Expert | Kinetis Expert

sdk.png

SDK is free, but you may need to supply some personal information including your name, email, company name, address and project description before downloading it.  Then you will get the page for downloading:

sdk2.png

Hope this helps! If not, could you please supply a screenshot to show the problem? And what are the steps to reproduce the problem? Thanks!

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,884件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello,

please, can you show us the printscreen of this message?

Do you mean downloading SDK into the board or from website?

Thank you.

Kind Regards,

Iva

0 件の賞賛
返信